Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the amperage ratings of a 9013G pressure switch?
Issue:
Will a 9013G switch handle 20A at 230V 1phase and 3HP?

Product Line:
Pressure Switches

Environment:
9013 Pressure Switches

Cause:
Will a 9013G switch handle 20A at 230V 1phase and 3HP?

Resolution:
The 9013G are not current rated devices. They are HP rated devices only. To use on 3 phase circuits, wire 2 phases through the 2 poles of the switch and direct wire the third phase to one of the motor leads. This makes the lead live when the pressure switch is OFF.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings