Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What operator handle is used with the 9422CSF30?
Issue:
What is catalog number for a 6" handle to be used with 9422CSF cable operators.

Product Line:
Operating Mechanisms

Environment:
9422 Cable operating Mech for Circuit breakers

Resolution:
Select 9422A1 for Nema 1, 3R, 4 and 12 or 9422A2 for Nema 4, 4X Stainless Steel enclosures

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings