Issue:
Needs the torque requirements for the terminal screws on the XB4/XB5 contact blocks.
Product Line:
Push Button and Operator Interface
Environment:
22 mm Push Buttons
Resolution:
The typical torque is 8.55 lb-in with a maximum torque of 10.7 lb-in.
Needs the torque requirements for the terminal screws on the XB4/XB5 contact blocks.
Product Line:
Push Button and Operator Interface
Environment:
22 mm Push Buttons
Resolution:
The typical torque is 8.55 lb-in with a maximum torque of 10.7 lb-in.
Released for: Schneider Electric Canada