How can we help you today?

What are the repair parts for a CU12L400FB, series M03?

Product Line:
CSEDs

Resolution:
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
Only the parts listed below are considered field replaceable.
Meter cover - 4056250650 (requires insulator and rivets, noted below)
Meter cover insulator - 4056138202 and rivets (2) 2430313190
Meter cover mounting screw - 4020513001K
Load center cover - 4056258950
Load center cover mounting screws - (3) 2142217101
Utility pullbox cover - 4056232801 (handles not included)
Utility pullbox cover handles - (2) 2940101103 and rivets (8) 2430315290
Utility pullbox cover mounting screws - (2) 4020513001K and sealing screws (3) X1299
Load center interior - 4056250750
Load center interior mounting screws - (2) 2142217101
Interior deadfront trim - 4056233001
Interior deadfront trim mounting screws - 4020513001K
Meter base assembly - 7329490250
Mounting channel - 4056142003
Factory installed main breaker - QDL22200
QDL main breaker mounting pan - 4056235201 and pan mounting screws (4) 2142720140
Utility lug mounting hardware - 4056211850
Semi-flush flange kit - FK400 (includes top endwall, top flange, and two side flanges)

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Help Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors