Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the replacement kit number for the ANSI Spring Discharge Interlock (DAE) shaft for the Masterpact NW breaker?
Issue:
Part number for the half-moon yellow (or silver) colored interlock shaft on the Masterpact NW Circuit Breaker

Product Line:
Air Circuit Breaker

Environment:
Masterpact NW Circuit Breaker

Resolution:
The replacement DAE kit number is S48554.
The bracket does not come with the kit; if replacing the shaft on an older breaker, it will be necessary to call Customer Service (Annie Brooks) in Columbia, SC to obtain the new bracket.

Schneider Electric Canada

Attachment(s)
S48554 Spring Discharge Shaft.png [173.88 KB]
S48554 - 48049-199-01.pdf [193.82 KB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings