Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Coil voltage selection for LU2B12 or 32 and LUB12 or 32?
Issue:
Why does the LU2B12 or 32 need a coil voltage selection while the LUB12 or 32 does not?

Product Line:
IEC Contactors and Starters

Environment:
TeSys U Open Motor Starter

Resolution:
The reversing LU2B12/32 has a coil in the reversing module so a coil voltage must be selected. The coil voltage of the non-reversing U line is determined solely by the control module.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings