Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the RXM2AB1BD contacts switch 28VDC?
Issue:
Can the contacts of RXM2AB1BD be switched to 28VDC

Product Line:
Relays and Timers

Environment:
RXM Plug-in Relay

Resolution:
Yes, nominal load (conforming to IEC, resistive, 100K cycles) is 12A at 28Vdc.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings