Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for an external auxiliary contact for NEMA type S Contactors & Starters?
Issue:
Identifying external auxiliary contacts for NEMA type S devices

Product Line:
NEMA Contactors and Starters

Environment:
8502/8536 Type S Contactors and Starters

Cause:
Need an external auxiliary contact

Resolution:
Class 9999SX6 for one normally open, 9999SX7 for one normally closed or 9999SX8 for one normally open and one normally closed. These contact units are externally mounted and are field convertible.

For additional auxiliary contact options see Auxiliary Contacts in the Class 9999 Accessories section of current Digest.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings