Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the CH364AWK, series F6? (may be shown as F06)
Issue:
Repair parts for CH364AWK, Series F6.

Product Line:
Safety Switches

Resolution:
The repair parts for the CH364AWK, series F6 (F06) are as follows. No other parts are available.
-Line Base Assembly - 4056703450 - (1 required - includes phynolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips if applicable)
-Line Base mounting screws - 4020546401 (2 required per line base)
-Load Base Assembly - 4056677450 (1 required per phase - includes phynolic base, lugs, and fuse clips)
-Load Base mounting screws - 4020546401 (2 required per load base)
-Arc Suppressor Assembly - 4056677550 (1 required per phase)
-Arc Suppressor mounting screw - 4020514501
-Lug Assembly - 4025116251 (per lug)
-Lug Assembly mounting screw - 2140122240 (per lug)
-Switch Mechanism - 4056678650 (also requires switch mechanism gasket 4056786001)
-Switch Mechanism mounting screws- 2299940562 (2 required)
-Handle Assembly - 4056663550 (also requires handle gasket 4056603101)
-Lockplate - 4056672101
-Lockplate mounting screws - 2299940562 (2 required)
-Equipment Ground Lug Kit - PKOGTA2

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Help and Contact Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings