Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for a CH365, series E2 and E4 heavy duty safety switch?
Issue:
Design repair parts

Product Line:
Heavy Duty Safety Switches

Resolution:
The parts listed here are the only field replaceable parts.
Complete interior - HN365E2 (includes line and load base assemblies, arc suppressor assembly, box insulator, line and load phase insulators, and mounting hardware)
Line base assembly - 4055218850 (3 required; arc suppressor assembly not included)
Load base assembly - 4055219050SEL (3 required)
Arc suppressor assembly - 4051270850SEL (3 required) obsolete replaced by 4051270850
Lug assembly - 4025113650 (1 required per base assembly)
Line base phase insulator - 4051201401 (2 required)
Load base phase insulator - 4055219101 (2 required)
Line and load base mounting screws - 4020600901 (2 required per base assembly)
Handle assembly - 4051217250SEL
Handle knob kit - 4028343550
Door thumb screw and retainer - 4405043401 and 4405049001

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings