Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why does the 9422TF3, 9422ATF13 and 9422ATF23 have 400A fuse clips? Is it 400A rated or 200A rated?
Issue:
200 A or 400 A rating of Fuse clips for 9422TF3, 9422ATF13 and 9422ATF23

Product Line:
Operating Mechanisms, Disconnect Switches, and Door-Closing Mechanisms

Environment:
Flange Mounted Disconnect Switches

Resolution:
This is a 200A fusible switch with 400A fuse clips. It still is a 200A disconnect with 200A horsepower ratings. Overfusing is permitted by the NEC and is sometimes required to accommodate the 175% rule when sizing the power fuses. Sometimes the upper horsepower ratings for a particular NEMA size category will result in requiring the next larger fuse size when the FLA of the motor is multiplied by 175%.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings