Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the deadfront part numbers for 225A, 42 circuit NQOD panels with a vertically mounted Q or K frame main breaker?
Issue:
Interior trim for the obsolete NQOD panelboards with vertically mounted Q or K frame mains

Product Line:
Obsolete NQOD Panelboards

Environment:
Products sold in North America

Resolution:
The available Main breaker deadfronts for the obsoleted NQOD panels are as follows:

SINGLE PHASE INTERIOR
(1) 80116-324-75 (Q FRAME MAIN BREAKER cover)
(1) Interior branch breaker deadfront is OBSOLETE

THREE PHASE INTERIOR
(1) 80116-324-75 (Q FRAME MAIN BREAKER)
(1) NQODRPL442L2 Interior breaker deadfront

The K frame Main breaker cover for both single and three phase has been obsoleted and is no longer available since 2018.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings