Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the acceptable mounting positions of the D-Line contactor?
Issue:
Mounting positions of LC1D contactor

Product Line:
IEC Contactors and Starters

Environment:
Tesys D Contactors

Cause:
What are the acceptable mounting positions of the D-Line contactor?

Resolution:
Normal mounting in relationship to the vertical plane. Devices can be rotated 180 degrees but cannot exceed +/- 30 degrees forward or backward from the vertical back plane.

Note: The deviation only applies to AC controlled devices; DC controlled devices will operate properly only when mounted in the normal position in regards to the vertical plane, i.e., do not rotate left or right from the normal upright and vertical position.

See attached file

Schneider Electric Canada

Attachment(s)
Operating position.pdf [134.02 KB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings