Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the catalog number for the bus finger or panelboard connector for the NQOB panel using the QOB breaker?

Article available in these languages: Spanish

Issue:
Using QOB Breakers, what is the panelboard connector for the NQOB Panels?

Product Line:
Panel boards

Resolution:
SK5668 is the bus finger or panelboard connector kit for use on the NQOB panel with QOB breakers. This is a 3 pole kit with A, B and C phase connectors. In a 225 A NQOB interior, this kit will allow you to mount 6 poles of breakers whether they are 1 pole, 2 pole, or 3 pole breakers. In a 400/600 A NQOB interior, this kit will allow you to mount 3 poles of breakers whether they are 1 pole, 2 pole, or 3 pole breakers.

Schneider Electric Canada

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings