Issue:
Repair parts
Product Line:
Canadian Heavy Duty Safety Switch
Resolution:
The repair parts for the CHU364RB, series F5 (F05) are as follows. No other parts are available.
Complete Line/Load Base - 4056703950 (1 required; includes the phenolic base, arc suppressors, lugs, rotor, and switching blades)
Line/Load Base mounting screws - 4020546401 (6 required per line base)
Arc Suppressor Assembly - 4056677550 (1 required per phase)
Arc Suppressor mounting screw - 4020514501
Lug Assembly - 4025116251 (per lug)
Lug Assembly mounting screw - 2140122240
Switch Mechanism - 4056678650 (also requires interlock shaft gasket 4056786001)
Switch Mechanism mounting screws- 2299940562 (2 required)
Handle Assembly - 4056663550 (requires handle gasket 4056603101)
Lockplate - 4056672101
Lockplate mounting screws - 2299940562 (2 required)
Cover latch and spring - one each of 4056607201 (latch) and 4022304301 (spring)
Repair parts
Product Line:
Canadian Heavy Duty Safety Switch
Resolution:
The repair parts for the CHU364RB, series F5 (F05) are as follows. No other parts are available.
Complete Line/Load Base - 4056703950 (1 required; includes the phenolic base, arc suppressors, lugs, rotor, and switching blades)
Line/Load Base mounting screws - 4020546401 (6 required per line base)
Arc Suppressor Assembly - 4056677550 (1 required per phase)
Arc Suppressor mounting screw - 4020514501
Lug Assembly - 4025116251 (per lug)
Lug Assembly mounting screw - 2140122240
Switch Mechanism - 4056678650 (also requires interlock shaft gasket 4056786001)
Switch Mechanism mounting screws- 2299940562 (2 required)
Handle Assembly - 4056663550 (requires handle gasket 4056603101)
Lockplate - 4056672101
Lockplate mounting screws - 2299940562 (2 required)
Cover latch and spring - one each of 4056607201 (latch) and 4022304301 (spring)
Released for: Schneider Electric Canada