Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do I obtain a replacement 8903 PB rectifier and coil?
Issue:
How do I obtain a replacement 8903 PB rectifier?

Product Line:
NEMA Contactors and Starters

Environment:
8903 Type PB lighting contactors

Cause:
How do I obtain a replacement 8903 PB rectifier?

Resolution:
The rectifiers are available as part of a kit which also includes the solenoid. These parts should be replaced as a set. The 9998PBV02 (120V), 9998PBV08 (208V), 9998PBV39 (240/277V), and 9998PBV28 (480V) are replacement coil & rectifier kits for these lighting contactors.


Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings