Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the CHU364AWK, series F6? (may be shown as F06)
Issue:
Current design repair parts

Product Line:
Heavy Duty Safety Switches

Resolution:
The repair parts for the CHU364AWK, series F6 (F06) are as follows. No other parts are available.
-Complete Line/Load Base (all one piece) - 4056703950 (1 required; includes phenolic base, arc suppressors, lugs, rotor, and switching blades)
-Line/Load Base mounting screws - 4020546401 (6 required per line base)
-Arc Suppressor Assembly - 4056677550 (1 required per phase)
-Arc Suppressor mounting screw - 4020514501
-Lug Assembly - 4025116251 (per lug)
-Lug Assembly mounting screw - 2140122240 (per lug)
-Switch Mechanism - 4056678650 (also requires interlock shaft gasket 4056786001)
-Switch Mechanism mounting screws- 2299940562 (2 required)
-Handle Assembly - 4056663550 (requires handle gasket 4056603101)
-Lockplate - 4056672101
-Lockplate mounting screws - 2299940562 (2 required)

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings