Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is needed to mount a GV2ME to a LC1D 09 to D32?
Issue:
What adapter or combination block to be used together with the LAD31?

Product Line:
Contactors and Starters-IEC

Environment:
Tesys GV Manual Starter and Protectors

Answer:
Either use a GV2AF3 combo block or a GV2AF4 block with LAD31 mounting plate . This later pair of parts will allow the front faces of the starter /protector and contactor to be aligned .

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings