Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is the GV7AP03 rotary handle lockable?
Issue:
GV7AP03 padlock provision

Product Line:
Tesys GV Manual Starter and Protectors

Environment:
North American Products

Resolution:
Yes, it has a feature to use up to 3 padlocks with a shank diameter of 5 - 8mm and can be locked in the OFF position only.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings