Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are XALD enclosures suitable for use outdoors?
Issue:
Need to know if they can use the XALD, XALK enclosures outside.

Product Line:
Push Buttons and Operator Interface

Environment:
XB4 and XB5 22 mm operators and enclosures

Resolution:
The XALD enclosures can be used outdoors.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings