How can we help you today?

What are the repair parts for an 82455, series A1 double throw safety switch?

Product Line:
Double Throw Safety Switch

Resolution:
The parts listed here are the only field replaceable parts.
Blade assembly - 4053859650 (4 required)
Top switch base assembly - 4053859550 (4 required)
Bottom switch base assembly - 4053859350 (4 required)
Base mounting screws - 2142718241 (2 required per base assembly)
Handle knob assembly - 4028435750
Lug assembly - 4025113651 (1 required per base assembly)
Keps nut for mounting lugs - 2342702200 (1 required per lug)

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: