Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can an I Line panel interiors be mounted horizontally instead of vertically?
Issue:
Verify if an I-Line panel interior can be mounted horizontally instead of vertically.

Product Line:
I-Line panelboard sold and supported in the USA.

Environment:
Installation

Cause:
N/A

Resolution:
No, breaker handle orientation would be opposite for half of the breakers and the interior heat rise would not be able to dissipate properly.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings