Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there a mushroom button that is momentary pull, maintained neutral, maintained push?
Issue:
Does Schneider offer a 30mm mushroom button that is momentary pull, maintained neutral, maintained push?

Product Line:
Pushbutton and Operator Interface

Environment:
30mm Pushbuttons

Resolution:
Yes there is the 9001KR8 and 9001SKR8 offer. Mushroom buttons with this operation were also available in the 22 mm XB2 line, a handful of these operators are still available.

Schneider Electric Canada
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings