Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the difference between a compensated and a non-compensated thermal overload?
Issue:
Compensated & Non Compensated overload

Product Line:
Contactors and Starters IEC

Environment:
IEC Overload relays

Resolution:
An ambient compensated bi-metallic overload relay is used where the controller is located in an area with a widely varying temperature and the motor is in an area (like a submersible pump well) that has a constant temperature. The non-compensated overload is used when the motor and overload are located in the same ambient area.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings