Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: What replaces an existing control transformer (ex: 9070EC1D9) or other open core and coil transformer in an MCC, starter, or OEM piece of equipment?
Issue:
Industrial Control Transformers

Product Line:
LV Transformers

Environment:
Applies to Low Voltage Transformers by SquareD/Schneider Electric

Cause:
Replacement of 9070 Control Transformers

Resolution:

The EC series of transformers is obsolete and can be replaced by either the 9070EO or 9070T lines of product.
The customer must contact the MCC or starter group, or the OEM for assistance.

This was an old leaded transformer with a thermal cutoff . Now use a 9070EL1D9 with secondary fusing.

The following video demonstrates how to differentiate Square D 9070 T, TF, and EL Series Control Transformers:

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings