Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can a LSDL label be used on a panelboard if 42 circuit directories are needed?
Issue:
LSDL label can be used on a panelboard if 42 circuit directories are required

Product Line:
Panelboards sold and supported in the USA.

Environment:
Installation

Cause:
42 circuit directory requirement

Resolution:
Yes. The LSDL label could be used for a panelboard.
Although normally used on a QO or Homeline Load Center, these stick-on labels could also be used on an NQOD, NQ or NF panel as well.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings