Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are the 8903 Type L and LX lighting contactors rated for use on motor loads?
Issue:
Are the 8903 Type L and LX lighting contactors rated for use on motor loads?

Product Line:
8903 type L and LX lighting contactors

Environment:
Products sold and used in the United States

Cause:
Are the 8903 Type L and LX lighting contactors rated for use on motor loads?

Resolution:
No. The 8903 Type L and LX lighting contactors are not rated for use on motor loads. Recommend using the 8502/8536 devices for motor loads or the 8903 type ``S`` lighting contactors, which are rated for motor loads, if they are in a mixed load situation.


Schneider Electric Canada

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings