Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Customer needs to know the resistance on a 31096-400-24, 480V coil for a size 5 Series A starter
Issue:
31096-400-24 resistant haracteristics

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Type S Contactors

Resolution:
15.5 ohms.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings