Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: What are the compression lugs for Powerpact H breakers?
Issue:
What are the aluminum and copper compression lug part numbers and wire ranges for the Powerpact H frame breakers?

Product Line:
PowerPact H frame breakers

Resolution:
These are the aluminum and copper compression lugs that are available for the PowerPacT H frame breakers, along with their wire ranges.
For (1) conductor #6 - #2 AWG Al or Cu Qty (3) part number is YA060HD.
For (1) conductor 1/0 - 4/0 AWG Al or Cu Qty (3) part number is YA150HD
For (1) conductor #6 - 1/0 AWG Cu only Qty (3) part number is CYA060HD
For (1) conductor #4 - 2/0 AWG Cu only Qty (3) part number is CYA150HD

The following video demonstrates the procedure for installing and wiring the YA060HD compression lug kit to PowerPacT H-Frame breakers:

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings