Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are the ZB4 and ZB5 contacts positive opening contacts?
Issue:
ZB4 and ZB5 force guided contacts

Product Line:
22 mm Push Buttons

Environment:
XB4/XB5 Electrical Components

Resolution:
The normally closed contacts are positive opening per EN 60947-5-1.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings