How can we help you today?

Do safety switches have a UL marine listing?

Product Line:
Heavdy Duty Safety Switch

Resolution:
Heavy duty, 30 - 200 A, NEMA 4/4X/5 (stainless steel) and NEMA 12/3R safety switches with UL marine listing are available as a special order. To get these switches, add suffix SLC to the catalog number of the switch and enter the switch as a special order. The SLC suffix means that copper phase/neutral/ground lugs (as applicable) are factory installed and there is a UL marine listing manifest added to the wiring diagram of the switch.