Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the lug wire range for an 800 amp main lugs I-Line panel?
Issue:
What are the conductor sizes for an 800A MLO I-line panel?

Product Line:
Panels

Environment:
I-line Products sold and used in the United States

Cause:
Product Features

Resolution:
The lugs on this panel will accept 4-#3/0 to 750kcmil Al/Cu per phase and neutral.  However, the conductors are limited to 3-#3/0 to 500kcmil Al/Cu per phase and neutral to conform to UL/CSA wire bending space.

Schneider Electric Canada

Explore more
Range:
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
Category:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings