Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is replacement coil part number 31041-400-49 available?
Issue:
Availability of coil 31041-400-49

Product Line:
Type S Contactors

Environment:
NEMA Contactors and Overload Relays

Resolution:
No. This coil was rated 208 to 220 volt 60 hertz and was used with Series A Class 8502 and Class 8536 Type SA_ contactors or starters only. To obtain the proper replacement use 31041-400-48 for 208 volt 60 hertz or 31041-400-51 for 220-240 volt 60 hertz control applications.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings