Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does a catalog number 9999RR04 remote actuator for MotorLogic overloads require external power, or is the power provided internally from the overload circuit?
Issue:
Does 9999RR04 remote actuator for Motor Logic overloads require external power, or is the power provided internally from the overload circuit?

Product Line:
NEMA Contactors and Starters

Environment:
Class 9999, 9065 Motor Logic solid-state overload relays (SSOLRs)

Resolution:
A 9999RR04 remote actuator for Motor Logic overloads is a coil or a solenoid that requires an externally switched source of 120V AC power. No control power is available from the overload itself.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings