Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does SquareD/Schneider Electric provide fuses for the primary and the secondary of a 9070 Type TF Industrial Control Transformer?
Issue:
Industrial Control Transformer fusing

Product Line:
LV Transformers

Environment:
Applies to Industrial Control Transformers by SquareD/Schneider Electric

Cause:
Fused Industrial Control Transformers, 9070TF type

Resolution:
No. While the 9070 Type TF Industrial Control Transformer comes with a 3 pole fuse block (2 rejection type Class CC fuses for the primary, and 1 non-rejection type midget fuse for the secondary,) SquareD/Schneider Electric does not provide the fuses. Proper fuse selection is the installer`s responsibility and is dictated by NEC table 450-3(b) and any specific application parameters that exist with any Industrial Control Transformer installation.


Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings