Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the catalog number of the 20a/1p branch breaker to be used in the obsolete NQOB panel rated 120/208, 3ph-4w, 10K AIC?
Issue:
20A 1 Pole breaker to be used on NQOB Panel rated at 120/208, 3ph-4w, 10K AIC

Product Line:
NQOB Panelboard

Environment:
Products sold and used in the United States

Cause:
Selection / Installation

Resolution:
Use the QOB120


Schneider Electric Canada

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings