Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for an RC2040M200CGP, series M01?
Issue:
Design Repair Parts

Product Line:
Combination Service Entrance Device

Resolution:
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only parts considered field replaceable:
Meter Cover - 4056167850 (includes latch)
Load Center Cover - 4056157550 (includes hinges and latch)
Load Center Cover Mounting Screws - (4) 2159417121
Dead Front Interior Trim - 4056173901
Dead Front Interior Trim Mounting Screws - 4020513001K (contains 10 screws; only 2 screws required)
Load Center Interior - 4056162050 (main breaker not included)
Load Center Interior Mounting Screws - (6) 2153217161
Main Breaker (Utility) - QOM2200VH
Main Breaker Mounting Hardware - (2) 2342702001 Keps Nuts
Main Breaker (Generator) - HOM230
Generator Interlock Kit - RCGK2
Meter Base Assembly - 4056190150 (includes meter base, line side lugs, line and load side meter jaws, line and load side meter jaw blade guides, and load side connector bussing)
Meter Jaw - (4) 7329794850
Meter Jaw Mounting Keps Nuts - (4) 2342702001
Meter Jaw Blade Guide - (4) 4052761901
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings