Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the EDB, EGB, or EJB breakers be used on 120 Vac system?
Issue:
Are EDB, EGB or EJB breakers rated for 120V system?

Product Line:
Miniature Circuit Breaker

Environment:
E Frame Breakers

Resolution:
Yes, those breakers will work on 120 Vac system.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings