Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are blank filler plates available for NQ panelboards?
Issue:
Blank filler plates for NQ panelboards

Product Line:
NQ Panelboard

Environment:
Maintenance

Cause:
Replacement

Resolution:
Yes. Catalog number is NQFP15, (shown on the individual plates as p/n 80122-005-01).
These are plastic, and sold in  package  Qty of 15 . They are approximately 2 1/2" W x 3/4" H x 1/2" D size.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings