Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What does the the ``2`` suffix designate at the end of part number LC1K1210B72?
Issue:
On part number LC1K1210B72, what does the last number "2" means?

Product Line:
Tesys K Contactor and Starter

Environment:
IEC Contactors and Starters

Resolution:
It is the code for a device with integral transient suppression. Both B7 and B72 coils are rated the same 24V, but the -B72 provides integral transient suppression.

Schneider Electric Canada

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
  • Help and Contact Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings