Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are NEMA 12 safety switches Mill Duty rated?
Issue:
Application

Product Line:
HD SS

Resolution:
In the past, Square D has used the term "mill duty rated" to describe our NEMA 12 safety switches that were provided with factory installed copper lugs. The current series switch does not come with copper lugs as standard. Copper lug kits are available for field or factory installation. For factory installation, add suffix SLC to the catalog number. Lexington will provide a letter if requested, self certifying the NEMA 12 switch with copper lugs as Mill Duty.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings