Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can busbars be replaced on the new NQ series panelboard interiors?
Issue:
Interior busbar part numbers for the NQ series panelboards

Product Line:
NQ Panelboard

Environment:
Maintenance

Cause:
Replacement

Resolution:
Replacement busbars for the interior, are NOT available.
Bus fingers / connectors, as they are called, is part number SKNQBC .
This is a 3 phase buss connector kit containing A, B and C phase connectors and mounting hardware.
This is for all amperage NQ panels.
bus

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings