Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the rail to snap down an EDB, EGB or EJB circuit breaker part number?
Issue:
Does Schneider offer replacement breaker mounting rail on NF panelboards? Can it be replaced without ordering an entire new interior?

Product Line:
NF Panelboards

Environment:
Products sold in North America

Resolution:
The part number 80113-002-01 is for a replacement rail for the branch breakers and can be ordered seperately instead of a complete new interior
edg

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings