What is the AIC rating of a QOB3125SL subfeed lug kit?
Issue:
SFL kit AIC or available interrupting capacity rating
Product Line:
Panelboards
Environment:
NQ Panelboard
Cause:
Product Features
Resolution:
The subfeed lug kit would carry through the existing AIC rating of the panel it is attached to. The breakers in the panel determine the AIC rating, not the lugs or hardware.
SFL kit AIC or available interrupting capacity rating
Product Line:
Panelboards
Environment:
NQ Panelboard
Cause:
Product Features
Resolution:
The subfeed lug kit would carry through the existing AIC rating of the panel it is attached to. The breakers in the panel determine the AIC rating, not the lugs or hardware.
Released for: Schneider Electric Canada