Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can a shunt trip be used with the QOM2 breakers used in a QOM22225N(F or S) or a QOM22225NRB enclosures?
Issue:
Product Design Features

Product Line:
QOM2 Circuit Breaker Enclosures

Environment:
Shunt trip accessory

Cause:
Application

Resolution:
Yes. The shunt trip for 120, 208 or 240V on a QOM2 type main circuit breaker is internal and factory installed ONLY and does not interfere with the fit of the breaker into these enclosures. Order the QOM2 main breaker catalog number with the suffix '1021'.  For example QOM2200VH1021.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings