Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the CH361AWC, series F7 (may be shown as F07)?
Issue:
Current Design Repair parts

Product Line:
Canadian Heavy Duty Safety Switches

Resolution:
The repair parts for the CH361AWC, series F7 (F07) are as follows. No other parts are available.
-Line Base Assembly - 4056603950 (1 required; arc suppressor not included)
-Load Base Assembly - 4056604150 (1 required)
-Line and Load Base Mounting Screws - 4020515101 (3 for line and 2 for load)
-Arc Suppressor Assembly - 4056635550 (1 required)
-Arc Suppressor Mounting Screw - 4020514501 (1 required)
-Lug Assembly - 4025101652 (per lug)
-Lug Mounting Screw - 4020514202 (per lug)
-Mechanism Assembly - 4056787350 (also recommend replacing switch mechanism gasket and handle gasket)
-Switch Mechanism Gasket - 4056786001
-Mechanism Washer - 2360200008
-Handle Assembly - 4056663550 (also recommend replacing handle gasket)
-Handle Gasket - 4056603101
-Lockplate - 4056672101
-Lockplate Mounting Screw - 2299940562 (2 required)
-Rod/Linkage Assembly - 4056787050
-Receptacle - 2541002806
-Receptacle Mounting Screws - 4510280101 (4 required)
-Ground Lug - 4025101652 (3 required)
-Ground Lug Mounting Screw - 4020513503 (2 required)
-Fuse Pullers - FPK03 (1 required)

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings