Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the time frame for a 9065 solid state Motorlogic overload relay - base or feature unit - to trip after a phase loss or phase failure?
Issue:
How many seconds would a 9065 solid state Motorlogic overload relay to trip after a phase loss or phase failure?

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Class 9065 Motor Logic solid-state overload relays (SSOLRs)

Resolution:
It should trip within 3 seconds on a complete loss of phase.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings