Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the maximum number of spaces and circuits catalog number CQO124M125C100, Series S04, load center will allow?
Issue:
Product Features

Product Line:
Canadian QO load centers

Evironment:
Total spaces-circuits

Cause:
Application

Resolution:
The maximum number of spaces using standard single pole breakers is 24 and the maximum number of circuits using QO tandem type breakers is 48.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings