Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are there Feed Through Lugs (FTLs) kits available for the NQ panelboards?

Article available in these languages: Spanish

Issue:
What are he part numbers for the Feed thru lug kits for the NQ panelboards?

Product Line:
NQ Panelboards

Environment:
Application

Cause:
Product features

Resolution:
Feed thru , Field installable lug kits are available :

For 225amp Interiors, 30 or 42 circuit interiors use a NQFTL2 kit.  For the 225amp, 72 or 84 circuit interior use a NQFTL2H.
For the 400amp interiors, 30 or 42 circuit interiors use a NQFTL4L. For the 400amp, 72 or 84 circuit interior use a NQFTL4H.
For 600amp interiors, feed-through lugs are only available on factory-assembled panelboards.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings