Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can a QO or Homeline load center be ordered with all copper neutral bars?
Issue:
What kind of material  is the neutral bar of QO or Homeline Center made of?

Produce Line:
Load Center

Resolution:
No. All load centers have aluminum neutrals as standard. Copper is not an option.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings